Hi!
I use a closedcube board with LMT70.
I connected LMT70 to a 12-bit ADC input to the NUCLEOF410RB board.
The problem is that for a constant temperature, I get an unstable value on the ADC and thus an unstable measured temperature.
The board on which the LMT70 is placed has 2 capacitors on it. (one decoupling 100nF and one filter capacitor 0.1nF).
I tried to power the whole system with a battery, also, I stabbed the sensor directly into the NUCLEO board (without wires), but none of that helped.
Can someone help me, how can I get a stable output?