Other Parts Discussed in Thread: TDC7200, TUSS4470, MSP430FR6047
Hi team,
While reading the datasheet of TDC1000 and TDC7200, I came across some doubts.
The datasheet says clearly the effect of the speed of water through the pipe on water measurement. But, nothing about the level of water in the pipe.
If the level of water flowing through the pipe is let's say 50%, the amount of water through the pipe will be entirely different when the water level flowing through the pipe is 90%.
How can we determine such a difference?.
Do we need additional sensors to sense the water level through the pipe?.
Awaiting your reply