Other Parts Discussed in Thread: OPT3001, OPT3004
Hi team,
I would like to ask some questions which are showing as below. I'm not familiar with ALS so question may be simple. Please help answer as detail as you can. Thank you very much.
1.
Measurements: 0.01 lux to 83 k lux
-> Does this mean the range is similar to eye diagram?
2.
23-Bit Effective Dynamic Range With Automatic Gain Ranging
-> What does this mean? Does it mean that we could transfer lux unit to digital signal unit and it has 2^23 step?
3. 12 Binary-Weighted Full-Scale Range Settings: < 0.2% (typ) Matching Between Ranges
-> what does this mean?
4. Could you help take an example if OPT3001-Q1 sense 10k lux? what will I2C of OPT3001 output?
5.
Rejects > 99% (typ) of IR
-> Does it mean the external IR wouldn't affect the OPT3001-Q1?
Regards,
Roy