Part Number: LDC1614
Other Parts Discussed in Thread: LDC1612,
Hello,
I am using two LDC1614s and one LDC1612 to detect the presence and positioning of a metal target.
The system sequentially enables one sensor at a time after putting the other two in standby (SLEEP_MODE_EN = 1).
An external crystal (40MHz) supplies the same clock to the three sensors.
The 10 LC sensors have the same layout, the same capacitor and are driven with the same current (AUTO_AMP_DIS = 1, RP_OVERRIDE_EN = 1 and DRIVE_CURRENT = 17). The measured frequency is very similar (~ 3MHz) as well as the conversion result (2037697 <DATAn <2049399 +/- 3 with OFFSETn = 0).
Now, if I select internal clock (REF_CLK_SRC = 0) the absolute values decrease due to the theoretical increase of the reference frequency (43.4MHz typ VS 40MHz). The values are similar for the two LDC1614 which go from just over 2 million to 1.8 million with the two DATA of LDC1612 which drops to just over 1.7 million. This, probably due to a higher value of the internal oscillator.
This not be a problem for the functioning of the sensor.
The problem is that the instability greatly increases with DATAn values that vary even by +/- 100.
Such unstable values of DATAn at rest and very different when approaching the target (same distance) are not acceptable for the functioning of the sensor.
Do you have an explanation or a suggestion that can solve?
I am available to provide further details.
thanks
Best regards,
Samuele