Other Parts Discussed in Thread: IWR1843, IWR1642
Hi I have purchased both the IWR1642 and the IWR1843 traffic monitoring demo, However the performence between these two are very different and so is the interface, here are the description of these discrepencies and some questions I have.
The IWR1843 demo in Industrial toolbox 4.5.1 detects a lot of objects that aren't cars espacially when I am moving with the radar , The screenshot below is when I put the radar stationary and having a car passing by, as you can see the passing of the car triggered the radar to detect a lot of different tracked objects that are neither there or moving. while it one of the tracked objects IS indeed the movement of the car, a lot of extra unwanted objects appears:
However for the IWR1642's demo in toolbox version 4.1.0, it doesn't detect any of the random objects as cars and only shows the actual cars, however it is not very reliable, as shown in the picture below it detects the car's orientation, however, the car should be a lot more to the left than its position on the picture:
I am wondering what exactly is causing such a discrepency between the two versions? are they using two different tracking algorithms, if so how are they different? Also how is it that the IWR1642 demo can see the orientation of the car while the IWR1843 can only see a circle as the car? And is it possible to have the IWR1843 demo's correct object pattern without all those unwanted falsely tracked objects?
Thanks!