This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMP117: TMP117 extended temperature & accuracy

Part Number: TMP117


Hi

TMP117 is defined for -55C...+150C operation. The temperature register however spans from -256C...+255C. I assume that I would thus get a temperature reading also at -80C?

I just want to read the temperature at -80C. will this device read the same or not?

If yes: what is the achievable accuracy in -80C... -55C?

If no: is the expected performance still linear in that range?

Also I just want to know the what is the time/duration to sense the change in temp using I2C lines?

Regards,

Manish Mistry