Hi, Staff
The datasheet has been updated from "L" to "M" on PCN (20201014001).
The recommended values for bypass capacitor and pull-up resistor have changed for the following update items.
• Changed bypass capacitor recommendation from 0.1uF to 0.01uF........22
• Updated recommened pull-up resistor size to standard 4.7kΩ ........22
1. I have been able to use it without any problems so far,
but is it okay to use the same value as before (is it okay if I do not change it)?
2. What could be the problem if I didn't change it?
best regards
cafain