Other Parts Discussed in Thread: AWR1843,
Hi,
I am using CAN SBL Lab on TI's Automotive Toolbox v3.2.0 on AWR1843 Boost Board.
1. I generated the binary using CCS and flashed to AWR1843 Boost Board.
2. After that, I opened Teraterm of the Data Port and changed the Baud Rate to 115200.
3. Pressed the Reset Button on AWR1843 Boost Board. After that i clicked Enter.
4. After that I clicked Space Button.
5. Opened the Command Prompt, Executed the CAN Metaimage Flasher with the Binary.
6. In the Command Prompt, It said File Sent.
7. But in Teraterm, It was showing Error: RPRC Parsing Failure.
Error Message :
Press any key to stop auto boot and Update Meta Image...
Loading existing Meta Image from Flash in 20 19
Debug: Update Meta Image selected
Debug: Device info: Manufacturer: 0, Device type = 0, Capacity = 0
flash address: c0000000
Debug: Loading application metaImage from Flash address: c0040000
Debug: Erasing SFlash...
Debug: Flash Erase complete
Debug: Start the image download using XMODEM over UART Or Hit 'Space Bar' to start Image download ove CAN interface
CCCDebug: Total data written = 0x39400
Error: RPRC Parsing Failure!!!
Can you suggest any idea to resolve the issue?
Regards,
Shankar.N