This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR1642BOOST

Other Parts Discussed in Thread: IWR1642

I found it  was difficult for me to download the source code of DSS and MSS with the instruction of users' guide of IWR1642 BOOST when  I want  to build the Demo lab. Pls refer to the feedback information asfollowing and let me  know how to make  it work.

  1. Furthermore, I want to know the best range resolution of the sensor of IWR1642 Boost regarding it will  be used to measure the human body for 生理特征. The necessary range resolution should  be less than 0.1mm. Can the sensor work for this purpose? Thank you!

  • Are you behind any proxy or VPN? This may be the reason why you are unable to download the package. However, this is not the only way to get the source code. You can also download the Industrial Toolbox as a zip and get the source code after extracting. Follow the readme for more instructions: https://dev.ti.com/tirex/explore/node?node=AOeX-yPbUcqy5W0kmizXEQ__VLyFKFf__LATEST 

    In terms of range resolution, the best possible range resolution is about 4cm.Regardless of your sub-millimeter requirement, I would still experiment with the IWR1642 and see if it matches your expectations.

    1. It didn't work either when  I tried the new link website. I also found this website is still the same link you sent to me before. At the same time, I checked my computer and found no VPN or proxy being installed. It would be greatappreciated if you can send me thesource code file directly.
  • I can not provide the source directly. Please explain and document (with as many screenshots as possible) the exact steps you are doing to download the package.

    Do you see the 3 dots by "Industrial Toolbox" and can you click download? Please follow all steps in the readme linked above.