In Firefox I can see the image on a post but not on the responses.
In Chrome I at least get a little icon showing that there is an image to view:
Is there a fix for this in Firefox?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
In Firefox I can see the image on a post but not on the responses.
In Chrome I at least get a little icon showing that there is an image to view:
Is there a fix for this in Firefox?
Hi John,
I'm seeing the same two screen shots in both Chrome and Firefox. What I don't see in Firefox is that small graphic you highlighted, but that seems to be an incorrectly pasted image, in other words, there is no image there to view, but an attempt to place it was made. When I click on it in Chrome, it's just a blank panel. Since it's blank, I suspect that is why Firefox doesn't show it.
Can you edit that post and attempt to upload the image again, please?
~Leonard
John,
Here's another clue: if I right-click on either of the 'scope shots in the other Replies, I have the option of downloading the image. The small blue icon, I cannot do this, as there is no image there.
~Leonard
Hi John,
One more update: that blue icon you see in the Chrome window, that is an indication of a timeout error when attempting an image upload. For some reason, Firefox does not have the same icon, but the results are clearly shown, there is no image displayed.
~Leonard
The original post shows the image properly. I can edit that.
The reply does not show the image. I can't edit the reply. Should I be able to edit a reply?
Clearing cookies and cache gave no improvement.
Hi John,
On the Reply, click MORE, then Edit. The text box will then be available for edit, try to paste the image in the box.
If you are unable to do this, click Reply to that same Reply you posted, upload the image into the new Reply box.
~Leonard
Thanks. I'd swear I just tried that and edit wasn't there! Now when I edit I see the 'image link' that you do:
I dragged a .png file in again and hit reply. The image shows properly in the email that gets sent to me, so it seems to be an issue with recalling it from the website afterwards.
If I edit again I can see the original broken link and the new image.
Another clue. When I edit a previous response I can select the 'broken link' icon and select 'convert to link'. When I do that and then attempt to load the link into Firefox I see "The Image <link name> cannot be displayed because it contains errors". Here's the link:
When I attempt to open this link in Chrome it doesn't show anything.
Hello John,
Thanks for the additional feedback. I will have to find an expert on this anomaly, so it may take a few days. I'll give you an update by Thursday this week.
~Leonard
Hi John,
I just looked at the thread again in Firefox, and I DO see the 'scope shot. It also shows you edited this Sep 29, so perhaps when you did that it uploaded the image. Be sure to clear Firefox browser cache and cookies, see what you can view after that:
~Leonard
p.s. and in fact the link you sent for the image, I clicked on it, at first nothing, but about 20seconds later, the image did appear:
e2e.ti.com/resized-image/__size/320x240/__key/communityserver-discussions-components-files/1024/7673.scope_5F00_1.png
I see it is working now too, without clearing cache and cookies. I just had to wait a couple of minutes and then reload the image.