This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV61070A: Output Voltage

Part Number: TLV61070A
Other Parts Discussed in Thread: TPS61023,

Tool/software:

Hi,

I have a question about TLV61070A and TPS61023.

Can these ICs fail if 5V is applied to the Vout pin when Vin=0V?

Looking at the absolute maximum rating, Vout (max) =7V, so I think it will not fail. Is this correct?

Best Regards,

Nishie