• Resolved

Need assistance modifying a thread

Prodigy 145 points

Replies: 4

Views: 46

Hello, 

I'd like to request for the last 2 posts in thread 2550605 to be deleted. The information is less than perfectly correct, and may be misleading if used as reference. 

https://e2e.ti.com/support/amplifiers/f/14/p/690782/2550605#2550605

Please let me know if this can be supported. 

Regards,
Vladimir

  • Can you tell me exactly which two?  The last answer was accepted as having solved the thread, so I'm hesitant to delete it.

    Bill Traynor
    E2E SysAdmin/DevOps

  • In reply to William Traynor:

    Bill - the very last two posts. The second to last asks an additional question, and the last post offers not fully accurate information as a response. I would advise deleting both in order to keep the thread accurate and complete at the same time. 

    Regards,
    Vladimir

  • In reply to Vladimir Ilic:

    OK, I've deleted them.

    Bill Traynor
    E2E SysAdmin/DevOps

  • In reply to William Traynor:

    Thank you Bill.