Hi team,
Does TI have a similar solution to ADG1411? thanks
P2P is better. or similar function
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Jimmy,
Yes we do have similar solutions - however our solutions that are similar to the ADG1411 typically have a better leakage current spec and are 1.8V compatible - but slightly more resistive - this difference is less than an ohm typically though.
That being said both the TMUX6211 and TMUX7211 are p2p replacements for the ADG1411. These parts are currently in preview and will be released to market soon - but the TMUX6212/TMUX7212 are currently available and the only difference is that they are logic high instead of logic low as with the ADG1411/TMUX6211/TMUX7211
If you have any other questions please let me know!
Best,
Parker Dodson