Hi team,
My customer is looking for MUX for multi-channel temperature sensor, and I’d like to ask your advice.
The system (for 1CH) would be like the one in TIDA-010019 with RTD sensor and Type K thermocouple.
There will be 12CH thermocouples, so they’d like to use two 12CH MUX, one for thermocouple +input and the other for thermocouple -input.
The switching speed from one channel to the next channel is slow (~1ms).
I’ve searched for 12CH MUX and there are only 3 devices, e.g. SN74CBTLV16292. Those are a little bit old, and I’m not sure if those are suitable for this application.
The customer values the cost most, so if the total cost is low, using multiple MUX with smaller channel number is also possible.
Could you provide recommendation for this application?
Best regards,
Kurumi