Other Parts Discussed in Thread: TMUX1204, TMUX1104, TMUX1109, TMUX1309
Dear Team,
I want to use TMUX6104 in one of my applications.
I have a single 5V supply available.
Will this IC work properly with a 5V supply.(VDD=5V and VSS=0V)
In the datasheet, I can see that "Wide Supply Range: ±5 V to ±16.5 V (Dual Supplies) or 10 V to 16.5 V (Single Supply)".
The absolute maximum rating is given below.

From these absolute ratings what I understood is it can work with VDD=5V and VSS=0V(GND).
Please correct me if I am wrong
Regarding
HARI