The TI E2E™ design support forums will undergo maintenance from July 11 to July 13. If you need design support during this time, open a new support request with our customer support center.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LV4052A: COM Line Voltage

Part Number: SN74LV4052A

Hi,

We are powering the IC with 3.3V. The select lines operate at this voltage.

Can we apply 5V on the COM pins?

  • Hi Akash,

    The short answer is no as the analog I/O pins are rated at VCC + 0.5V (with input voltage limited to 5.5V max) - so for your system 3.8V - and you the max voltage passed should be approximately ~VCC (so if 3.6V were input a max of 3.3V should show on the output)

    The long answer is maybe - 

    From the abs max table in the datasheet - the max switch I/O voltage has 2 notes. Note 2) "The input and output negative-voltage ratings may be exceeded if the input and outpu current ratings are observed" - Since there are diodes to ground and VCC on the I/O pins they will conduct at ~0.5V above the VCC voltage - they have a max current of 50mA through them. So if the input signal is going to be greater than VCC + 0.5V, a series resistor is needed in front of the mux input to essentially exchange voltage for current but there is some resistance in the diode so less current is always a better option if this is the way you want to move. So you can - but I wouldn't recommend it as it opens up more possible problems - but as long as the current into those diodes is limited to 50mA so that the device can actually clamp to ~VCC + 0.5V on the input there shoulnd't be much of an issue.

    If you have any other questions please let me know!

    Best,

    Parker Dodson