Because of the holidays, TI E2E™ design support forum responses will be delayed from Dec. 25 through Jan. 2. Thank you for your patience.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMUX1136: Simulation Model

Part Number: TMUX1136
Other Parts Discussed in Thread: TMUX1119

Hello Support Team,

I'd like to add TMUX1136 to my Hyperlynx signal integrity simulation and I'm looking for the best simulation model.

Looking at the link below, it seems that a simple RC is suitable to model the device.

https://e2e.ti.com/support/switches-multiplexers-group/switches-multiplexers/f/switches-multiplexers-forum/986756/tmux1574-max-propagation-delay

Anyway I'm wondering if the C_ON capacitance reported on the datasheet (page 8) need to be added twice (before and after the resistor, as better explained in the picture below)

Many thanks,

regards,

Massimiliano

  • Hi Massimiliano,

    Before I get into the passive modeling tips on a mux - I would like to point you to the TMUX1119 (As we have PSpice / TINA spice models for it). The results won't be perfect but both devices are from the same low voltage precision family - the biggest difference is the TMUX1119 is only 1 channel - but its impact on the signal is very similar to the TMUX1136 and will probably give a better approximation than a passive model - at least for room temperature -(so if you go above 25C it will give a baseline but it won't be super accurate) with all that being said I think the TMUX1119 model + a higher temp passive model can get a decent approximation of how to expect the device to work in the system. 

    that being said you are correct - for quick general channel impact simulations to help get some boundary condition approximations you can use a simple model.

    On your second question, C_ON is the effective capacitance of the switch (when closed) from input/output to ground. This means the C_ON of 20pF for the TMUX1136 only needs to be added once as you have shown in option 1.

    However a passive model using option 2 is a better passive model - but the capacitances won't both be 20pF. The S side of the device (S pins) will have a capacitance to ground of CS_Off - which for the TMUX1136 at VDD = 3.3V is 6pF. (I am assuming 3.3V supply due to the resistance being worst case for the +85C range.). The other side would be CD_OFF + C_Switch - which isn't spec'd for the TMUX1136 directly but can be found by C_ON - (CS_OFF) = CD_OFF + C_SWITCH (this approximation holds for many of our switches but not all - but for the TMUX1136 this approximation is ok) So  either of the following models would be okay (Assuming 3.3V supply at -40C to 85C range":

    If you have any other questions please let me know!

    Best,

    Parker Dodson

  • Hi Parker,

    many thanks for your detailed answer !

    Regards,

    Massimiliano