Hi,
Could you please let me know if TMUX1104DGSR is a Pin to Pin replacement for MAX4734EUB. If not, what is the best replacement device you can recommend.
Regards,
Sandesh
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Could you please let me know if TMUX1104DGSR is a Pin to Pin replacement for MAX4734EUB. If not, what is the best replacement device you can recommend.
Regards,
Sandesh
Hi Sandesh,
The TMUX1104DGSR is in same package/pinout as the MAX4734EUB and there are some parametric differences.
These can be summarized as follows:
Ultimately the parts can work in similar applications as they both are precision and while they aren't 1:1 the TMUX1104 still has great performance on these specs, is our closest option for a cross, and realistically the largest gap of applications I see is ones where continuous current requirement is higher than 30mA - but we don't have a similar pin to pin device that matches this devices continuous current.
If you have any other questions please let me know!
Best,
Parker Dodson