Part Number: TMUX7462F
1. Considering that the typical impedance of a CAN bus is 120Ω, is the maximum on-resistance of 16Ω an issue? My customer designs the system considering the minimum impedance of CAN can reach 60Ω and manifested concern in using the TMUX7462F. Do we have extensive data results for CAN networks? I understand the 16-Ω only occurs at 125°C, but does that mean for CAN the temperature range has to restricted?
2. DS section 8.3.2.4 recommends tying Vfp to Vdd and Vfn to Vss if fault supplies aren't available. Section 10 however suggests a sequence and voltage ramp of Vdd and Vss prior to Vfp and Vfn respectively. Can you comment on why connecting the pins together is not an issue?
Thank you!