Other Parts Discussed in Thread: TS3A27518E, SN74CB3T3257
Hi Team,
Whether TS3A27518E-Q1 could achieve logic and also achieve level shift at the same time?

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Team,
Whether TS3A27518E-Q1 could achieve logic and also achieve level shift at the same time?

Hey Amelie,
The TS3A27518E (and all other TI analog multiplexers / switches) are passive and will just provide a path when the channel is selected that gives an equivalence of a 4.4ohms (typ). It will not behave as a level shifter. So if you're trying to drive the 1.8V SDIO port signal to both the 3.3V and the 1.8V memory card then you will need an extra level shifter before the 3.3V device.
Thanks,
Rami