This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TS3DS10224: Layout impedance suggestion for USB2.0 application

Part Number: TS3DS10224


Hi team,

My customer is using our TS3DS10224 for usb2.0 application.

They would like to consult with the layout impedance range of TS3DS10224  in USB2.0 application.

I didn't see it at datasheet. Would you suggest to follow as below? Thanks.

USB 2.0 differential impedance: 90 ohms +/- 15%

  • Hi Feng,

    It is best to follow the advised differential impedance requirements of the protocol you are using in the application as the TS3DS10224 will not be impacted by this as it acts as a passive switch that passes the signal from input to output with minimal distortion.

    Thanks!

    Bryan