Part Number: TMUX1133
Other Parts Discussed in Thread: TMUX1574
Hello team,
Is it possible to use the TMUX1133 for switching SPI?
Regards,
Carlo
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Carlo,
The TMUX1133 could certainly be an option for SPI switching if you just need to switch 3 out of the 4 typical SPI signals and only need up to 220MHz of bandwidth. Our typical recommendation for this application is usually our TMUX1574 which is a 2:1x4 multiplexer with extremely high bandwidth which can work with virtually any SPI application.
Let me know if you have any further questions on this.
Thanks!
Bryan