Part Number: SN74CB3T3245
Hi team,
On the datasheet of SN74CB3T3245, it is mentioned that “All unused control inputs of the device must be held at VCC or GND to ensure proper device operation.”.
Which pins are the control inputs?
At first I thought those are A1~A8, but I found this thread. Are A&B pins I/O pins and OK to left floating? And by control pin does it mean OE-pin?
If the A1~A8 are the control pins, then, when A1 and B1 are not used, only A1 should be connected to Vcc/GND? Or, Both A1 and B1 should be connected to Vcc/GND?
Best regards,
Kurumi