Dear Team,
Could you kindly help me suggest TI solution for TK22A10N1
if CSD19537Q3 or CSD19534KCS possible or not?


This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear Team,
Could you kindly help me suggest TI solution for TK22A10N1
if CSD19537Q3 or CSD19534KCS possible or not?


Hello Victor,
Thanks for the inquiry. The TK22A10N1 is in a TO220 isolated fullpak (plastic tab) package. Our closest cross to this FET is either the CSD19533KCS (lower on resistance: 10.5mΩ max vs. 13.8mΩ max at VGS=10V) or the CSD19534KCS (higher on resistance: 16.5mΩ max at VGS=10V) in a standard, non-isolated (metal tab) TO220 package. We do not make any FETs in an isolated TO220 package.
Best Regards,
John Wallace
TI FET Applications