Other Parts Discussed in Thread: TMUX1248, , TS5A3159
What is the dB loss through the switch? There is nothing in the data sheet that gives this information. Normally there would be a curve showing the loss vs frequency. The data sheet says input a signal with a 0.4V bias applied and increase frequency until the -3dB point is observed. This is not acceptable as I do not have a part on hand. I am considering using it, but without the loss figure I will have to rule it out.
I plan to use the device from 1-30 MHz.