Hi Expert,
To check datasheet for SN74CB3Q3257DBQR, and it states the Vih Min is 1.7V and Vil Max is 0.7-0.8V. I wanted to confirm that this is only for “control input” (OE and select pins), and not for data I/O ports?

On the first page it also says that 0.8V and 1.2V are supported for data I/O, but still I would like to make sure that 1V application in the data I/Os is ok.

Regards,
Mark