Other Parts Discussed in Thread: TMUX6208, TMUX1108
Hi,
is there any device have same package with ADG1608BCP? Thx
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Ruixin,
We do not have a matching 3mm x 3mm QFN packaged device.
The TMUX6208 has the same pinout but its package is 4mm x 4mm WQFN and it doesn't support the lower 3.3V supply voltage ranges.
The TMUX1108 has the same pinout and supports the lower voltage ranges. It is offered in a 1.8mm x 2.6mm UQFN package.
Thanks,
Tyler