Part Number: SN3257-Q1
Other Parts Discussed in Thread: UCC21710, , SN74LVC1T45-Q1, SN74LVC1G3157-Q1, SN74LVC1G97-Q1, SN74CB3T3257, TXU0104-Q1
Hi,
We are looking at using SN3257-Q1 as a multiplexer and voltage level shifter. The input is from a microprocessor (TMS570) and a seperate hardware safety circuit (for FUSA) - the mux logic is used to determine which input line is passed through to a UCC21710 gate driver. The input parts operate at 3,3V whereas the gate driver is on a 5V rail.
In our design the input signals are 0-3,3V (low-high logic) - the outputs are to the gate driver UCC21710 which requires (we believe 5V input on the gate drive signal live - datasheet shows minimum of 70% of VCC (ie. 0.7x5V = 3,5V).
Is there a design adjustment we can use to satisfactorily lift the input signal from 3,3V all the way to 5V or at least adequate to robustly drive the IN+ line on the gate driver.
In all respects we were very attracted to SN3257-Q1 as the datasheet implied that a 1.8V input could be output at 3,3V however we are not clear on this now.
Thanks,
John