Other Parts Discussed in Thread: TMUX7209
Hi team,
My customer is using ADG409BRZ. I find our P2P device is MUX509 but the supply is 36V which is lower than ADI part. Do we have other suitable devices to replace it? Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Yuting,
The TMUX7209 is p2p and has a higher voltage rating than the MUX509. It is the correct cross for the competitor's device.
We are currently refreshing the BOM crosses for our portfolio so there shouldn't be mismatches like this in the future.
Thanks,
Tyler
Hi Tyler,
Thanks for your reply. I see ADG409BRZ is SOIC package and TMUX7209 has TSSOP and WQFN. It is not p2p for ADG409. Do we have SOIC device with high voltage rating? Thanks.
Hi Yuting,
Sorry I missed the SOIC part of the cross. The MUX509 is the highest rated SOIC packaged 4 channel 2:1 that we offer.
Please confirm the power supply configuration that the customer uses. The +/- 22V dual power supply configuration looks to be the gap between the devices. If the customer doesn't use +/- 22V, then the MUX509 would be a good option.
Thanks,
Tyler