Part Number: TS5A23166
Other Parts Discussed in Thread: TS5A21366
e2e,
I would like to replace TS5A23166DCUR with T5A21366DCUR. Would you please let me know the pinout, package, and parametric differences between these two devices?
Thank you,
Adam
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hey Adam,
These devices are pretty similar but there are slight spec differences in CON and leakage specs. They also share the same pinout and the packages are the same as well. The biggest differentiation here will come in the logic levels. The TS5A23166 looks to be using some TTL logic compatible levels:

While the TS5A21366 has the upgraded feature of being 1.8V logic compatible:

For more information on the VIH, VIL levels and 1.8V logic compatibility we have a couple good resources i'm linking below as well:
[FAQ] What are the VIH & VIL Levels of an Analog Switch / Multiplexer
Application Brief : 1.8 V Logic for Muxes and Signal Switches
Hope this helps!
Thanks,
Rami