This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMUX6219: can vdd be connected to pin 12 (NC)?

Part Number: TMUX6219


Team,

I'm posting on behalf of my customer.

The datasheet indicates that pin 12 has “No internal connection. Can be shorted to GND or left floating”.  Since there is no internal connection on pin 12 can I connect this pin to VDD (+5.4V) without any issues?

Thanks,

Tom