Hi,
I found that TS5A3359 in my case can be right part for blowing MSP430 fuse, but have some questions.
In device absolute maximum ratings there is 6.5 VCC max, but it is not clear to me if device can switch 6.5V (Analog voltage) on VNO and VCOM? Or absolute maximum analog voltage is 5.5V?
For fuse blow 6V 100mA during 1ms is used. Out of this period (99.9% of life time) device will be on 4.5V VCC.
Also want to know real benefit from leaving device off (VCC=GND), except current consumption.