This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74CBT16210C: ON resistance when Vin=3.3V or Vin=5V when VCC=5V & usage of multiple ports in parallel

Part Number: SN74CBT16210C
Other Parts Discussed in Thread: TPS22919, SN74CBTLV3861, TMUX1511, SN74CB3Q16211

The datasheet did not have the ON resistance value or chart to show when Vin=3.3 and Vin=5V @VCC=5V. Can someone tell me the resistance number? Thanks.

In addition, please advise whether my below approach is achievable or not. Thanks.

Plan to use this switch to pass 5V (500mA) to the next-level PCB as VDD of this next-level PCB. As this switch's absolutely maximal ON state switch current is 128mA, can I use 4 or 5 ports (128mA x 4 > required 500mA) in parallel to choose whether this 5V (500mA) should be pass or not? If yes, I can also minimize the effective ON resistance due to parallel connection.

The single incoming wire will be connected with 4 (or 5) input ports, use _OE to decide whether to pass or not, and 4 (or 5) related output ports will be connected with a single outgoing wire, which is the VDD of the next-level PCB.