Other Parts Discussed in Thread: TS5A3167
Hi team,
Customer ask if SN74LVC1G66 can support power down protection which means that there is no problem even if the voltage hots the terminal when the power is off.
Best regards, ny
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi team,
Customer ask if SN74LVC1G66 can support power down protection which means that there is no problem even if the voltage hots the terminal when the power is off.
Best regards, ny
Hi NY,
SN74LVC1G66 does not have the powered off protection feature so it cannot have voltage on the terminals when the the device is powered off.
A similar 1 channel 2:1 configured mux with this feature is the TS5A3167.
Thanks,
Tyler