Other Parts Discussed in Thread: CD4051B,
E2E,
I was searching for an 8:1 mux and I see there is new product TMUX4051. What is the difference between the TMUX4051 and the traditional CD4051B?
Thank you,
Adam
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Adam!
This is a great question.
The TMUX4051 8:1 one-channel multiplexer is a p2p compatible upgrade to its predecessor CD4051B. TMUX4051 offers superior electrical performance compared to CD4051B.
TMUX4051 offers a wide single/dual supply range of 3V - 24V (+/-12V). Also, TMUX4051 offers 1.8V logic compatible inputs, which helps to support systems that utilize lower voltage rails.
One of the major break-throughs with the TMUX4051 is the package technology.
In addition to industry standard QFN (BQB) package, TMUX4051 offers the SOT-23-THIN (DYY) package type which is 57% smaller than the 16-Pin TSSOP package!
This allows the SOT-23-THIN package footprint to fit within the TSSOP package footprint, making it easy for layout implementation.
Regards,
Tyler