Hi Team,
As title, do we have device to replace UPG2214TB,which is a is a GaAs MMIC L, S-band SPDT (Single Pole Double Throw) switch? Thanks.
Regards,
Hailiang
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Team,
As title, do we have device to replace UPG2214TB,which is a is a GaAs MMIC L, S-band SPDT (Single Pole Double Throw) switch? Thanks.
Regards,
Hailiang
Hi Hailiang,
So this is an RF switch and our devices do not specify some of the typical characteristics a normal RF switch datasheet does (such as Insertion loss and different frequencies, return loss, loss compression, etc.).
However, the closest device we can recommend to this would be our TMUX136 device. It is a 2:1x2 channel device, but will be able to pass frequencies similar to the competitor device. For the extra channel, you can just terminate the inputs/outputs to GND through a 50 ohm resistor.
Thanks!
Bryan