Other Parts Discussed in Thread: TMUX7219, TMUX6219
Hi Team,
Our customer is worried about current Consumption increase.
Because, they referenced the application note(SCDA011) below.
https://www.ti.com/lit/an/scda011/scda011.pdf
They use TS12A12511 at the conditions.
I guess that TS12A12511 does not have the same problem as SCDA011.
So, I understand that positive supply current is 1mA(max) (does not reach the “mA” order).
Is my understanding correct?
[Conditions]
-Single Supply(Vcc pin) is 9V
- Logic control input(IN pin) is 3.3V
- Input signal is 8.5V(max)
Regard,
Hide