データシートの仕様を見ますとVIHが2.0V以上となっていますが、こちらの電圧はVCCの値とは関係ないでしょうか?
例えばVCCが2.0V~5.0Vで変動をした場合でもVIHは2.0V以上となりますでしょうか?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
データシートの仕様を見ますとVIHが2.0V以上となっていますが、こちらの電圧はVCCの値とは関係ないでしょうか?
例えばVCCが2.0V~5.0Vで変動をした場合でもVIHは2.0V以上となりますでしょうか?
This device is designed for a nominal 5 V supply. The VIH limit applies over the entire range, even in the worst case of VCC = 4 V.
Hello,
This device can handle VCC voltages from 4V-5.5V. When operated in that VCC range, you will need to provide a VIH of at least 2V for the device to register the input as a logic high.
Thanks!
Bryan