Part Number: TMUX8212
TMUX8212 looks like it has potential for professional audio. Can you specify THD+N under the following conditions?
±15V or ±18V
10KΩ and 100KΩ load
10Vpp and 20Vpp
20Hz to 20kHz BW
Alternatively, a plot that would capture all of this nicely would be Vrms vs. THD+N for a given supply voltage and load, like any op amp data sheet. You already have the 1KΩ data. It's especially relevant because of this note, in section 9.3.2: "The flattest on-resistance region extends from VSS to roughly 5 V below VDD. Once the signal is within 5 V of VDD the on-resistance will expoentially increase and may impact desired signal transmission." OK, so...can you show us that graphically?