Hi Team,
I have a question about the Spice model of TMUX1574.
I am simulating TMUX1574 with PSpice for TI.
When VDD voltage = 5V, it works as per the datasheet, but when VDD voltage = 3.3V, it doesn't work.
(Input signal is not output)
The datasheet states that the power supply voltage range of TMUX1574 is 1.5V to 5.5V.
The TMUX1574 should also work at 3.3V.
Is this a typo in the datasheet?
Or is there a problem with the Spice model?
In addition, the Spice model uses the one that comes with PSpice for TI.
Best regards.