Dear TI
We use TMUX1574PW item.
Does it matter if the IO voltage input from the MUX IC is different?
Below Picture is Possible?
S1_A - 1.8V
S1_B - 3.3V
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear TI
We use TMUX1574PW item.
Does it matter if the IO voltage input from the MUX IC is different?
Below Picture is Possible?
S1_A - 1.8V
S1_B - 3.3V
Dear Ladisch
Thank you your Feedback
I have question.
In our design, Supply voltage and Signal voltage are same. Is it possible?
As I know, in your document, if 3V powered, Signal range is 0V ~5.5V.
Thanks
Taegon.Kim
Yes, this is possible. (The TMUIX1574 allows even larger signal voltages than other switches.)