Hello,
regarding the TS5A3359 analog mux,
is there a "safest way" to have no-glitch on COM during power-up?
E.g. assume the COM options should be passing either 5V, 3.3V or 0V (GND) to COM (depending on IN1 and IN2).
So VCC has to be 5V and the 3.3V should be generated from the 5V supply (3.3V ramp later than the 5V ramp).
Now when the power-up default setting should be to pass 0V to COM and we don't want to see any voltage level >0V on COM during power-up,
would the best option be having the 0V at the NO2 input and to have pull-ups to VCC (5V) on IN1 and IN2?
There doesn't seem to be any kind of UVLO, so may the switch briefly turn on NO0 or NO1 to COM during the VCC ramp-up (even with having 5V pull-ups on IN1 and IN2)?
Thanks