This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN3257-Q1: Is SN3257-Q1 ok for RGMII switch?

Part Number: SN3257-Q1

Hi BU team 

Is SN3257-Q1 ok for RGMII switch function?  If it is not ok, would you help promote the right part ? This is an automotive application and need Q-grade device.

Thanks 

  • Hi Ted,

    What version of RGMII is being used? Also, what frequency is being used? Since there are multiple versions of RGMII I want to make sure I am looking at the same RGMII standard as the customer.

    Thanks!

    Alex

  • HI Alex

    The version of RGMII is 2.0 and the frequency is 125Mhz. 

    What's your comments?

    Thanks 

  • Hi Ted,

    From a strictly spec standpoint, this switch can handle the application in question. I would like to note we do have an ethernet team that may have more specialized devices depending on your overall system requirements. So, if you find you need something in that field then I would recommend reaching out to them for a recommendation as well!

    Thanks!

    Alex