Other Parts Discussed in Thread: TMUX1209
Hi team,
There are several questions about TMUX4051 and TMUX1209:
1. Can the two chips be used in UART signal when the maximum baud rate is 115200bit/s?
2. What's the meaning of bandwidth in the datasheet?
3. Are the two chips available as long as the frequency of protocol-type signals (SPI, SGPIO, UART, etc.) are within this bandwidth?
Best Regards
Silvia Gao