This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMUX6208: Swithing AC Voltage Signal

Part Number: TMUX6208

Hi,

I have 21 V AC (Maximum) Signal in my system. I have used a resistor deivider to reduce the voltage to 3 V AC as my Input VDD voltage to TMUX6208 is 3.3V DC. VSS is connected to -3.3V DC.

Can I feed 3V AC signal to Any source pin of TMUX6208 as it is a AC Signal.

Thanks.