This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMUX646: Ibis file

Part Number: TMUX646


Can you point me to the IBIS file for the TMUX646?

  • Hello David,

    We do not have an IBIS model for the TMUX646 currently only a S-parameter model will that work? 

    S-parameter models are more commonly used for high speed devices such as the TMUX646 since they provide more accurate results above ~1GHz.

    You can simulate an IBIS model in whatever IBIS software they're using by using the following circuit, which should be a good representation when the switch is on:

    Will this cover your model needs? If you need a more detailed IBIS model or a representational circuit when the switch is off please let us know. 

    Thanks,

    Nir