Other Parts Discussed in Thread: TS5MP645,
Dear Sir,
in our application we need to connected two MIPI cameras of 2 lanes to our i.mx8 processor. At a time only one camera shall be accessed by the imx8.
1)can we connect two cameras on same differential signals to i.mx8. i.e. MIPI clk from imx8 connected to both camera (in Y topology)?
2) if above is No , then which part is best suited to connect two cameras to imx8(Accessed one at a time)
3)what is the longevity of TMUX646 and TMUX645
4)what are the difference between TMUX646 and TMUX645