This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMUX1136: spec check

Part Number: TMUX1136
Other Parts Discussed in Thread: TMUX1574

Hi

This TMUX1136DGSR, does the customer want digital? Analog is more expensive

The requirement is 2:1 2 groups or 2:1 4 groups VCC 3.3V The customer's application is to switch SPI 4 wire and general uart, I2C, 220MHZ, which is enough

  • Hello,

    So all TI analog switches are can be used to pass analog or digital signals!

    In addition the TMUX1574 is a better device that can support 3.3v vcc, SPI 4 wire, uart and i2c. Also its bandwidth  is 2GHZ which means it can support a 200 MHZ signal.

    Please Take a look into our mux selection guides to learn about the protocols you have mentioned.

    Regards,

    Kameron