Hi,
The customer has the following problems when using this chip, please help to analyze.
1. When CTL2_6234=0 and CTL3_6234_EN#=0, VDDA=VDDA2=13.5V, U9 is off, but the voltage measured at D1 pin1 is 13.5V.
2. When CTL2_6234=1 and CTL3_6234_EN#=0, VDDA=VDDA1=20V, U11 is off, but the voltage measured at D2 pin1 is 20V.
It looks like TMU6234 was not fully disconnected from S1A and S1B after the switch.
The attachment is schematic design.
Thanks~