Hello, in the datasheet the Vdd current is specified as 72uA and Vss is specified as 30uA. Does that depend on the amount of flowing through the source or drain pins? Meaning if I have an application that is pulling 100mA through the switch, will the Vdd or Vss current increase?
I have an application where I'm using qty. 20 of the TMUX6221 and want to ensure that I'm designing the power supply adequately.
Thanks,
Derek